cancel
Showing results for 
Search instead for 
Did you mean: 

Is ST25RU3993 module support "Any Sensor tags " like RF micron ..?

Ssubr.1
Associate II

Hi ,

Is ST25RU3993 module support "Any Sensor tags " like RF micron ..?

1 ACCEPTED SOLUTION

Accepted Solutions
Cedric Dalban
ST Employee

Hello SSubr,

first of all, happy new year and all the best for 2021.

The ST25RU3993 module supports all tags fulfilling the ISO 18000-6 Type C specifications (aka Gen2) as well as GB/T 29768-2013 specifications (aka GBT29768) at all frequencies from 860 MHz to 960 MHz.

So, as soon as the sensor fulfills one of these specs, the ST25RU3993 will handle it ;-)

best regards,

Cedric.

View solution in original post

1 REPLY 1
Cedric Dalban
ST Employee

Hello SSubr,

first of all, happy new year and all the best for 2021.

The ST25RU3993 module supports all tags fulfilling the ISO 18000-6 Type C specifications (aka Gen2) as well as GB/T 29768-2013 specifications (aka GBT29768) at all frequencies from 860 MHz to 960 MHz.

So, as soon as the sensor fulfills one of these specs, the ST25RU3993 will handle it ;-)

best regards,

Cedric.