2020-03-11 09:41 AM
Hello,
I am trying to read some NFC tag with a X-NUCLEO-NFC03A1 attached to a NUCLEO F091RC board. I am a beginner into those technology, so basically I was trying to load the sample "NFC Detect " from the package "X-CUBE-NFC3" wich can be found on ST official website to understand how to use NFC stuff. The problem is, I tried to build the project on the STM32 IDE Cube, and it worked fine, but i can't read anything on the NFC NUcleo's antenna after running the programm.
I suppose there are problems of initialisation , but i have no idea how to debug this.
Thanks you for your time,
Best Regards,
Karim
Solved! Go to Solution.
2020-03-23 08:34 AM
Hi Brian ,
Yes it's my fault, I wasn't very clear about my explications. Thanks to you now I have more knowledge about RFID to explain my situation :
Regarding the T2T issue ;
According to the NFC tool android application, it's an NXP MIFARE Ultralight- NTAG 213
But i don't understand how you manage to find the Control lock TLV on adress 16, because when I study the data sheet , it's only for user memory :
https://www.nxp.com/docs/en/data-sheet/NTAG213_215_216.pdf
Regarding the M24LR (T5T)
After formating from X PACKAGE application, and write through X PACKAGE application too, i can read on the android application :
And the memory :
Then i tried to modify the message and read back the memory again :
And when I try to read it back on the X PACKAGE application, it's working fine :
But, i am now trying to understand why the adress n°05; 06; 07 has changed when i modified the message.
Thanks,
Best regards,
Karim
2020-03-24 01:54 AM
Hi Karim,
for T2T: as per the NFC Forum Technical Specification T2T v1.0, different TLV can be present after the Capability Container: Null TLV, Lock Control TLV, Memory Control TLV, etc.
For the M24LR, the NDEF TLV starts at address 4:
For more information, see:
Rgds
BT
2020-03-30 01:01 AM
Hello Brian,
Thanks you for all your informations . I have a lot more understanding of the hardware and software, i will come back for any further questions 🙂
Best regards,
Karim
2020-04-27 04:27 PM
Hello Brian,
For the final step on my project with those elements, i would like to adress specific value on memory blocks of the M24LRE EEPROM. According to this document, it exist function avaible to do such : https://www.st.com/resource/en/application_note/cd00271422-developing-your-m24lr64-r-datalogger-application-for-temperature-acquisition-stmicroelectronics.pdf
But I can't find ST IDE compatible projects to experiments this functions. Do you know if there is any example available on ST IDE ?
To be more clear, i need to learn how to write on the EEPROM memory blocks, to interact with an another application, wich answer depending on the EEPROM memory blocks value.
I am still using nucleo F091RC and NFC03A1 to interact with the M24 tag.
Best regards,
Karim
2020-04-28 01:03 AM
Hi,
M24LR is a dual interface EEPROM:
ST25R95 <--- RF ---> M24LR <--- I2C ---> MCU
On RF side, the M24LR64E-R follows the ISO/IEC 15693 standard and the physical memory is organized in block of 4 bytes. Due to memory capacity, the read/write commands (such as Read Single Block/Read Multiple Blocks, Write Single Block or Write Multiple Blocks) have been extended to support 2-bytes block address. This is supported through the following RFAL API in rfal_st25xv.c:
Rgds
Bruno
2020-05-04 01:06 AM
Hello Brian (Bruno ? )
Thanks you again for those very precise informations. It was exactly the functions I was looking for. But i am encoutering some problems with the arguments of the functions (especially with UID and FLAG arguments) . Would it be possible to get an example of the rfalST25xVPollerM24LRReadSingleBlock and rfalST25xVPollerM24LRWriteSingleBlock functions ?
It's the final step on my project.
Best regards,
Karim
2020-05-04 02:53 AM
Hi,
see demoNfcv() in demo.c for example of how to set UID and flag parameters.
Basically
uid = nfcvDev->InvRes.UID and flag = RFAL_NFCV_REQ_FLAG_DEFAULT
Rgds
BT
2020-05-11 08:35 AM
Hello,
Thanks you again for your advice. I studied the rfal_st25xv.c librarie to understand how I could manage to read and write into the memory blocks. As you noticed me, the demoNfcv() as been created to do so. I tried to use it,I copied/pasted it to the ndef_demo.c file, because i can't run it from the demo.c file (wich has been like excluded from the project) :
I am still using the M24 tag, so I am calling the function at the right place, when an ISO15693 has been detected.
As you can see i have put the demoNfcv function.
And now i got a read block error, but no error code is returned, so i can't understand why it is failling :
Best Regards,
Karim
2020-05-11 10:43 AM
Hi Karim,
the demoNfcv uses rfalNfcvPollerReadSingleBlock() whereas a M24LR64 tags has a extended block number coding.
rfalNfcvPollerReadSingleBlock() works for standard ISO15693 tags whereas rfalST25xVPollerM24LRReadSingleBlock has to be used for M24LR64 or M24LR16 tags.
If you want to read a block from a M24LR16 or M24LR64 tag, you just need to replace rfalNfcvPollerReadSingleBlock by rfalST25xVPollerM24LRReadSingleBlock in the demoNfcv.
Rgds
BT
2020-05-12 07:10 AM
Hello Brian,
I tried to replace rfalNfcvPollerReadSingleBlock() by the rfalST25xVPollerM24LRReadSingleBlock function. Here in the code (ndef_demo.c) :
I added a static variable with the asked structure :
And I just replaced the demoNdef(nfcDevice) originally in the code by the demoNfcv() .
No error or warining during compilation, but when I am trying to read through the application, still got read block fail :
Best regards,
Karim