cancel
Showing results for 
Search instead for 
Did you mean: 

CE/RED-testing of design with ST25R3911B

cha2
Associate

Hi,

We have designed a board based on ST25R3911B and it is about to be tested by a Notified Body with regards to RED/EMC.

In relation to this, I am wondering if there is ready-made SW available, that can be used for setting the radio to transmit a single tone on a given channel? It is needed as part of the RED-testing.

 

Br,
Chato

1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi Chato,

not exactly sure about your question. NFC is 13.56MHz only - no different channels available.  Emitting a "tone": Just enable the field.

Or do you have different requirements?

BR, Ulysses

View solution in original post

1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi Chato,

not exactly sure about your question. NFC is 13.56MHz only - no different channels available.  Emitting a "tone": Just enable the field.

Or do you have different requirements?

BR, Ulysses