cancel
Showing results for 
Search instead for 
Did you mean: 

What are max operating input voltage of vn7000ay logic pins (e.g. SEn, IN, SEL)?

jsmith
Associate II

I can't find the max operating voltages of the logic pins.  Is it same as Vcc?  Thanks.

1 REPLY 1
TDK
Guru

5V. Above that they're going to start clamping the voltage. See Table 9 in the datasheet.

 

TDK_0-1701738451026.png

 

If you feel a post has answered your question, please click "Accept as Solution".