cancel
Showing results for 
Search instead for 
Did you mean: 

Using MPP on stwlc38

Jvan .23
Associate II

Is it possible to use a Qi2 rx coil with magnetic array on a stwlc38 design?

The goal is to use a Qi2 charger and reap the benefits of magnetic alignment and 15W charging while still being on the Qi1.3 standard of the stwlc38.

1 ACCEPTED SOLUTION

Accepted Solutions
willzhou
ST Employee

Dear Customer

STWLC38 doesn't support Qi 2.0 spec, but Qi2 rx coil can be used.
So you can use Qi2 rx coil and magnetic to do 15W QI 1.3 power transfer.

More information about STWLC38

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
willzhou
ST Employee

Dear Customer

STWLC38 doesn't support Qi 2.0 spec, but Qi2 rx coil can be used.
So you can use Qi2 rx coil and magnetic to do 15W QI 1.3 power transfer.

More information about STWLC38

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
willzhou
ST Employee

We plan to release MPP stamp module, do you consider it?

willzhou_1-1724145874869.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jvan .23
Associate II

Interesting. If we would have to start over the project (so the layout was not done already) we would definitely consider it, also depends on pricing.

Dear Will

we are doing QI1.3 RX with magnetic but the progress is not going smoothly, and the time is limited, we must go ahead anyway.

and also will be going to make mpp standard RX, can you send me more information , thanks

 

TJ