hello sir I am using the fast transmission mode of the nfc chip ST25DV04KC to transmit picture data. The NFC chip is used with the MCU of STM32G071G8U6. When I write the 25KB picture data through the mobile APP into the NFC cache, I find that ...
Hellothanks for you kind reply.The writing time of 11 seconds is the actual measured time, even if it is reduced to the theoretical time of 7.7 seconds, it is a bit long. If I want to shorten this time to less than 4 seconds, does ST have any other F...