User Activity

Is it possible to use a Qi2 rx coil with magnetic array on a stwlc38 design? The goal is to use a Qi2 charger and reap the benefits of magnetic alignment and 15W charging while still being on the Qi1.3 standard of the stwlc38.
I have this board with a large (91x119mm) surrounding it. There is circuitry including the ST25R95 in the middle, but it has quite some clearance to the antenna. Matching network is calculated using the ST excel sheets.Now I can get it to read NFC st...
The datasheets front page mentions "Reader/Writer" as operating mode, but later only mentions " NFC-A / ISO14443A reader mode". Could you confirm that ISO14443A writing is supported?