cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SPIN3202 Connection failed!

PKhal.2
Associate

Hello, everyone!

Faced with such a problem with STEVAL-SPIN3202. Does not start the engine, when trying to connect it writes:

"Connection failed! No response, check the communication cable, the power on the board or the baudrate (set to 115200 bps)."

In Keil IDE writes that everything is OK. The firmware is installed.

LEDs on the board show that everything is OK.

Thanks in Advance!

Best regards,

Parviz

1 ACCEPTED SOLUTION

Accepted Solutions
Enrico Poli
ST Employee

Hello @PKhal.2​ ,

I think the problem is the mismatch between the speed set into the FW configuration (3rd screenshot) and the one set in the monitor (1st screenshot).

Please check if setting 9600bps in the monitor solves the issue.

Enrico

View solution in original post

2 REPLIES 2
Enrico Poli
ST Employee

Hello @PKhal.2​ ,

I think the problem is the mismatch between the speed set into the FW configuration (3rd screenshot) and the one set in the monitor (1st screenshot).

Please check if setting 9600bps in the monitor solves the issue.

Enrico

Cristiana SCARAMEL
ST Employee

Hello @PKhal.2​ 

did you solve your connection problem?

If yes please "Select as Best" the answer to help the Community.

If you feel a post has answered your question, please click "Accept as Solution"