cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32WB5MMG] Client role fails to connect to any server

BBute.1
Associate II

Hello,
I am using a STM32WB5MMG on a custom board for a BLE application. I started the project with the Client profile. The application is able to scan and receive advertisement frames. I use a MAC filter to select on peripheral and try to connect to it. As soon as I try to connect to the server with the function aci_gap_create_connection, the program enters an infinite loop inside hci_cmd_resp_wait. The response of this particular HCI command is never received.
I don't think it is related to bad parameter value such connection interval because I already faced this issue and in this case the function aci_gap_create_connection was returning an accurate error code.

RTC is on LSE, wakeup is activated, IPCC interrupts are enabled, RFWKP is on LSE.
As suggested in another post, I monitore the SR flash register and SRAM2A first register to see if CPU2 entered Hardfault but it does not seem to.

I changed a bit hci_cmd_resp_wait and hci_cmd_resp_release to provide a timeout in case no reply is ever get from CPU2:

 

 

 

void hci_cmd_resp_release(uint32_t flag)
{
  HW_TS_Stop(timeout_ts_ID);
  UTIL_SEQ_SetEvt(1 << CFG_IDLEEVT_HCI_CMD_EVT_RSP_ID);
  return;
}

void hci_cmd_resp_wait(uint32_t timeout)
{
  HW_TS_Start(timeout_ts_ID, MS_TO_TICKS(timeout));
  UTIL_SEQ_WaitEvt(1 << CFG_IDLEEVT_HCI_CMD_EVT_RSP_ID);
  return;
}
static void TimeoutHCI(void)
{
	LOG_WARNING("Timeout");
	/* Affichage de l'état du coeur 2 voir AN5289 rev 18 p 40 s*/
	uint32_t* ptr = SRAM2A_BASE;
	LOG_DEBUG("FLASH_SR  CPU2 Keyword   CPU2 Link Register CPU2 stack pointer");
	LOG_DEBUG("0x%08lX  0x%08lX  0x%08lX  0x%08lX  0x%08lX",FLASH->SR,*ptr, ptr[1],ptr[2],ptr[3]);
	hci_cmd_resp_release(0);
}

 

 

 

 Below is a light trace ouput to show the problem:

Spoiler

[app_entry.c][APPE_SysUserEvtRx][363] Wireless Firmware version 1.20.0

[app_entry.c][APPE_SysUserEvtRx][364] Wireless Firmware build 2

[app_entry.c][APPE_SysUserEvtRx][365] FUS version 1.2.0

[app_entry.c][APPE_SysUserEvtRx][367] >>== SHCI_SUB_EVT_CODE_READY

[app_entry.c][APPE_SysEvtReadyProcessing][453] >>== WIRELESS_FW_RUNNING

[app_entry.c][APPE_SysEvtReadyProcessing][477] >>== DBGMCU_GetRevisionID= 2003

[app_entry.c][APPE_SysEvtReadyProcessing][482] >>== DBGMCU_GetDeviceID= 495

[app_ble.c][APP_BLE_Init][319] Success: SHCI_C2_BLE_Init command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][751] ==>> Start Ble_Hci_Gap_Gatt_Init function

[app_ble.c][Ble_Hci_Gap_Gatt_Init][764] Success: hci_reset command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][778] Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET

[app_ble.c][Ble_Hci_Gap_Gatt_Init][779] Public Bluetooth Address: 00:80:e1:27:9c:7c

[app_ble.c][Ble_Hci_Gap_Gatt_Init][792] Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET

[app_ble.c][Ble_Hci_Gap_Gatt_Init][805] Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET

[app_ble.c][Ble_Hci_Gap_Gatt_Init][818] Success: aci_hal_set_tx_power_level command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][831] Success: aci_gatt_init command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][867] Success: aci_gap_init command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][906] Success: aci_gap_set_io_capability command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][934] Success: aci_gap_set_authentication_requirement command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][949] Success: aci_gap_configure_whitelist command

[app_ble.c][Ble_Hci_Gap_Gatt_Init][952] ==>> End Ble_Hci_Gap_Gatt_Init function

[app_ble.c][APP_BLE_Init][352] Success: aci_hal_set_radio_activity_mask command

[app_ble.c][APP_BLE_Init][354]

[p2p_client_app.c][P2PC_APP_Init][169] -- P2P CLIENT INITIALIZED

[app_ble.c][Scan_Request][972]
** START GENERAL DISCOVERY (SCAN) **

[...]

[DBG] main:164 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] main:165 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]-- GAP GENERAL DISCOVERY PROCEDURE_COMPLETED

** CREATE CONNECTION TO SERVER **

[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1092 >Timeout]
[DBG] TimeoutHCI:1095 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1096 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]

And then below is the full trace with the following debug parameters:

 

 

 

 

#define TL_HCI_CMD_DBG_EN 1 /* Reports BLE command sent to CPU2 and the command response */

#define TL_HCI_CMD_DBG_RAW_EN 0 /* Reports raw data BLE command sent to CPU2 and the command response */

#define TL_HCI_EVT_DBG_EN 1 /* Reports BLE Asynchronous Events received from CPU2 */

#define TL_HCI_EVT_DBG_RAW_EN 0 /* Reports raw data BLE Asynchronous Events received from CPU2 */


#define TL_MM_DBG_EN 1 /* Reports the information of the buffer released to CPU2 */

 

 

 

Spoiler

[DBG] SVCCTL_App_Notification:634 >Rx adv from 8C:A6:82:E0:00:10]
[tl_mbox.c][OutputDbgTrace][700] mm evt released: 0x3E
[tl_mbox.c][OutputDbgTrace][701] buffer addr: 0x20030238
[tl_mbox.c][OutputDbgTrace][705]

[tl_mbox.c][OutputDbgTrace][758] ble evt: 0x3E
[tl_mbox.c][OutputDbgTrace][761] payload: 02 01 04 01 C8 1D E7 CB 9A 35 00 9F
[tl_mbox.c][OutputDbgTrace][776]

[tl_mbox.c][OutputDbgTrace][700] mm evt released: 0x3E
[tl_mbox.c][OutputDbgTrace][701] buffer addr: 0x20030200
[tl_mbox.c][OutputDbgTrace][705]

[tl_mbox.c][OutputDbgTrace][767] ble evt: 0xFF
[tl_mbox.c][OutputDbgTrace][768] subevtcode: 0x0407
[tl_mbox.c][OutputDbgTrace][771] payload: 02 00 00
[tl_mbox.c][OutputDbgTrace][776]

[app_ble.c][SVCCTL_App_Notification][430] -- GAP GENERAL DISCOVERY PROCEDURE_COMPLETED

[tl_mbox.c][OutputDbgTrace][694] mm evt released: 0xFF
[tl_mbox.c][OutputDbgTrace][695] subevtcode: 0x0407
[tl_mbox.c][OutputDbgTrace][696] buffer addr: 0x20030200
[tl_mbox.c][OutputDbgTrace][705]

[app_ble.c][Connect_Request][995]
** CREATE CONNECTION TO SERVER **

[DBG] Connect_Request:1001 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] Connect_Request:1002 >0x00000000 0x20030028 0x20030048 0x20030058 0x20030078]
[tl_mbox.c][OutputDbgTrace][710] ble cmd: 0xFC9C
[tl_mbox.c][OutputDbgTrace][713] payload: 20 03 20 03 00 10 00 E0 82 A6 8C 00 28 00 50 00 00 00 F4 01 10 00 10 00
[tl_mbox.c][OutputDbgTrace][716]

[WARNING] TimeoutHCI:1096 >Timeout]
[DBG] TimeoutHCI:1099 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1100 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1096 >Timeout]
[DBG] TimeoutHCI:1099 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1100 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]
[WARNING] TimeoutHCI:1096 >Timeout]
[DBG] TimeoutHCI:1099 >FLASH_SR CPU2 Keyword CPU2 Link Register CPU2 stack pointer]
[DBG] TimeoutHCI:1100 >0x00080000 0x20030028 0x20030048 0x20030058 0x20030078]

Any help on this subject would be greatly appreciated. 

 

1 ACCEPTED SOLUTION

Accepted Solutions

After deeper investigations, we managed to fix the issue, though I do not understand clearly why, the issue disappears if RNG is deactivated OR "clock error detection" in RNG is disabled.
I do not think that we will require RNG module in our project, so I am fine to live with this.

Any insight regarding the reasons behind would still be appreciated.


Best regards

 

 

 

View solution in original post

6 REPLIES 6
BBute.1
Associate II

Up.

Sorry about this but we are stuck on this for a couple of months..

STTwo-32
ST Employee

Hello @BBute.1 

Could you try to reproduce this behavior on the STM32WB5MM-DK.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

I already did and I got the exact same behaviour.

Thanks for your help,

Best regards,

STTwo-32
ST Employee

Hello @BBute.1 

For more investigation I've escalated your request internally (under internal ticket number 196955). We will try to be back to you ASAP.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Joe_
ST Employee

Hi BBute.1,
I've just done the test on my side with a “p2pClient” on the STM32WB5MMG starting from release v1.20.0.
I don't reproduce the problem you encountered.
Would it be possible for you to share with us your project running on DK please?

BR, Joé

After deeper investigations, we managed to fix the issue, though I do not understand clearly why, the issue disappears if RNG is deactivated OR "clock error detection" in RNG is disabled.
I do not think that we will require RNG module in our project, so I am fine to live with this.

Any insight regarding the reasons behind would still be appreciated.


Best regards