2024-07-07 06:37 AM
Hello everyone,
I'm working on a circuit for monitoring the bias voltage of a GM tube, which requires a high voltage of 100V. I am currently using a OA1NP22C op-amp configured as a unity-gain buffer to read the divided voltage. To minimize current consumption, I'm considering using a voltage divider with 1GΩ and 12MΩ resistors. However, this configuration still consumes approximately 9.8µA, which is higher than I would like for my low-power application.
Here is a simplified version of my circuit:
My questions are:
Any insights, suggestions, or examples of similar implementations would be greatly appreciated!
Thank you!
Feel free to ask for further details if needed.
Zaim
2024-07-07 07:07 AM
Please check your idea again:
It would be better if you could insert schematics as a picture, including the opamp, so that we can make suggestions for improvement.
Regards
/Peter
2024-07-07 08:54 AM
Hi Peter,
Thank you for your feedback. You are correct about the current calculations.
To clarify, R1 is 1GΩ and R2 is 12MΩ. Please find the schematic below for further reference.
Regards,
Zaim
2024-07-07 09:01 AM
Hi Again Peter,
Regarding the voltage divider, the mentioned values were just a preliminary idea. The voltage divider network will only be used once a day to check the output voltage is stable, so it should not consume unnecessary current to help preserve the device's battery.
Regards,
Zaim
2024-07-07 09:35 AM
Peter little mix M and G, but still divider current is around 98nA for your values. Then seems uA current is from MCU and OP. Your point 2 is one step use NFET transistor and remove capacitor.
2024-07-07 09:44 AM
Hi MM,
Thank you for your insights.
Could you please illustrate any drawing or a schematic showing how the NFET will be used? Additionally, could you recommend a specific NFET or provide important considerations to check when choosing one?
Thank you for your support.
Regards,
Zaim
2024-07-07 09:44 AM
Hi,
>How can I further reduce the current consumption of this voltage divider to the nanoampere range?
You are there... 100V/1Gohm = 100nA . (100nA x 100V = 10uW - where you wanna go then ?
+ How much uA needs the cpu and all other circuit ? )
>Would switching out the voltage divider using a transistor be a viable solution?
Yes. But to get lower than 100nA, you only could use a mosfet; but at your 3v3 supply, only few mosfets can work at >100V and be switched with < 3V at the gate - so close to impossible.
2024-07-07 09:51 AM - edited 2024-07-07 10:56 AM
<removed because OP made it clear he's not a precocious 14 year old playing with fire>
2024-07-07 10:21 AM
Hi AScha.3,
Thank you for your insights, I understand your points exactly. Finding a small MOSFET with a low gate voltage is indeed challenging. Therefore, I still think that the voltage divider solution may be the best for our product. I also realized that I miscalculated the current; it should be 89nA, not 9.8uA.
An important consideration for our product is cost, and as you may know, GΩ resistors are very expensive. Thus, the maximum resistance I can use is 1GΩ. So, the question is: are there any other ways to achieve lower current consumption for this circuit, or should we proceed with the current values?
As I mentioned earlier, I will enable the ADC for this feedback once a day. I was considering completely shutting down the circuit and only powering it when I need to read the values. However, if the switching circuit draws more than 100nA, it might be hard to used, and I might have to use the configuration with the 1GΩ / 12MΩ resistors.
Thank you for your support.
Regards,
Zaim
2024-07-07 10:38 AM
I mean 98nA with transistor off can be reduced only to DS leakage current for example BSS123N
and is temp sensitive. Primary reduce other corrents.