2023-01-12 2:44 AM
According to the datasheet of the powerstep01 driver, a minimal baudrate of 5MHz has to be respected for the SPI interface. Is there any technical reason for that or can a lower (lets say <1MHz) baudrate be used for communication?
Solved! Go to Solution.
2023-01-12 5:10 AM
In fact, the data sheet is somewhat misleading at first glance because it does not state the
but rather the
as mentioned by Cristiana.
Regards
/Peter
2023-01-12 5:00 AM
Hello @pf8645 and welcome to the ST Community.
The 5 MHz is the Maximum SPI clock frequency - see powerSTEP01 datasheet at page14.
So you can use a SPI clock frequency lower than this value.
Let me know if I solved your doubts, if so please "Select as Best" label.
2023-01-12 5:10 AM
In fact, the data sheet is somewhat misleading at first glance because it does not state the
but rather the
as mentioned by Cristiana.
Regards
/Peter
2023-01-12 5:55 AM
Thanks a lot for the answers, I was indeed a bit confused by the datasheet, since the max frequency is stated in the "min." column.