cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I red the manual for UM2516 (B-G431B-ESC1). It states it can be connected with a LiPo S3 to S6. The specification however states voltages up to 60 V. Is it possible to use a LiPo S10 or is there another development board which I could use instead ?

MLagh.1
Associate
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Cristiana SCARAMEL
ST Employee

Hello @MLagh.1​ and welcome to the ST Community.

The B-G431B-ESC1 is designed for drones with up to 6S LiPo battery pack or equivalent suitable DC supply (6S LiPo battery pack have a nominal voltage of 22.2 V, 25.2 V fully charged voltage).

The "60 V" is the power MOSFETs voltage rating.

So you cannot use a 10S LiPo with this discovery kit.

The ST portfolio offers several reference designs, but the maximum supply voltage is up to 6S LiPo battery pack.

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

If you feel a post has answered your question, please click "Accept as Solution"

View solution in original post

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @MLagh.1​ and welcome to the ST Community.

The B-G431B-ESC1 is designed for drones with up to 6S LiPo battery pack or equivalent suitable DC supply (6S LiPo battery pack have a nominal voltage of 22.2 V, 25.2 V fully charged voltage).

The "60 V" is the power MOSFETs voltage rating.

So you cannot use a 10S LiPo with this discovery kit.

The ST portfolio offers several reference designs, but the maximum supply voltage is up to 6S LiPo battery pack.

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

If you feel a post has answered your question, please click "Accept as Solution"