cancel
Showing results for 
Search instead for 
Did you mean: 

L6470H discovery Issues on two systems

sburr
Associate II
Posted on October 02, 2014 at 22:29

I am attempting to run the L6470H discovery kit with the dspin software from a machine with windows xp on it. I was previously able to run it from another machine with xp, I installed the same files but cannot connect to the board. I get a windows error with the following parameters:

EventType : clr20r3     P1 : gui.exe     P2 : 1.2.5071.18356     P3 : 528b2b58

P4 : mscorlib     P5 : 2.0.0.0     P6 : 4a7ce2b8     P7 : 1295     P8 : 14    

P9 : system.missingmethodexception    

On the other system I get an error with spi_dll when I connect, any ideas?

I have tried to download the latest software with no luck.

#l6470h #discovery-eval6470-disc
2 REPLIES 2
Enrico Poli
ST Employee
Posted on October 03, 2014 at 16:03

Hi,

The SPINFamily software is based on the Microsoft .NET framework.

Please, check the installation of this component.

Regards

Enrico

sburr
Associate II
Posted on October 03, 2014 at 18:21

I installed 4.0 and I get the same error, this time it is delayed by a few minutes. do I need to install a different version of .net?