2022-01-20 11:32 AM
2022-01-21 2:29 AM
Welcome, @dave239955, to the community!
Footprints are typically included in newer datasheets, but unfortunately this is still missing here. In the meantime, ST has a cooperation with UltraLibrarian, which is also referred to via the CAD Resources tab, but unfortunately the footprint for the PPAK 5L in connection with the LF50ABPT-TR is still missing, too.
Workaround: the LDFMPT-TR also uses an absolutely identical package, so you can use its footprint even if it is a different LDO. Simply select tab CAD Resources and get the footprint from there.
Is that helpful?
Regards
/Peter
2022-01-21 2:29 AM
Welcome, @dave239955, to the community!
Footprints are typically included in newer datasheets, but unfortunately this is still missing here. In the meantime, ST has a cooperation with UltraLibrarian, which is also referred to via the CAD Resources tab, but unfortunately the footprint for the PPAK 5L in connection with the LF50ABPT-TR is still missing, too.
Workaround: the LDFMPT-TR also uses an absolutely identical package, so you can use its footprint even if it is a different LDO. Simply select tab CAD Resources and get the footprint from there.
Is that helpful?
Regards
/Peter
2022-01-21 6:35 AM
You can get footprints at
Paul
2022-01-21 3:14 PM
Thatnk you paul sadly PPPAK is not available from Mouser, or SnapEDA, the DPAK D2PAK versions are
2022-01-21 3:15 PM
thanks Peter that did the trick
2022-01-24 4:49 AM
--deleted--
2022-01-24 5:07 AM
Please don't use the footprint from the document on bdtic.com as it is from 2004 and much older than the current one mentioned above.
Regards
/Peter