2024-07-15 1:13 AM
Hello,
I have developed my own evaluation Board for the STWLC98 Chip. When connecting the power suplly, the DC-Mode, which is on the IC when it is delivered, works in a correct way. But when I want to program the IC with the following firmware from the ST Website:
STEVAL-WLC98RX_config_2C00.memh
STEVAL-WLC98RX_nvmpatch_1454.memh
I get the following errors, when the programming status bar reaches 100%:
Config Id Mismatch! file/chip: 0x2C00/0x1000
Wrong config id 0x1000 and patch id 0x0000 for RX
Where can I find the right Firmware or do you have any solutions for me?
Thank You
Simon
Solved! Go to Solution.
2024-07-16 1:07 AM
I have found the problem. The Output Voltage of the ft260 was 3.2V but the STWLC98 only supports 1.8V.
Thank you for the answers.
2024-07-15 1:21 AM
Hi Simon
Seems your evaluation Board have some i2c issues,
do you change anything from EVK sch board?
Does chip I2C pins well welding?
Also you can use this tool "wlc_ft260_Recovery.7z" to erase chips.
Wireless Charging solution Wiki - STMicroelectronics Community
If you can show GUI log to us, it will be better.
2024-07-15 1:51 AM
Hi Will
The schematic is the same.
The I2C Chip seems to be welded well.
The wlc_ft260_Recovery tools works fine.
But there is still the same problem when loading the firmware to the board
I have sent you the txt log file via private message.
2024-07-15 2:12 AM
2024-07-16 1:07 AM
I have found the problem. The Output Voltage of the ft260 was 3.2V but the STWLC98 only supports 1.8V.
Thank you for the answers.
2024-07-16 1:09 AM
yes, we suggest follow ft260 dongle sch and add level shift ic.