cancel
Showing results for 
Search instead for 
Did you mean: 

Binary flashing script

GHM
Associate II

How to flash a binary file to the microcontroller with script only ie without STM32Cube IDE & Stm32cube programmer. Please provide a detailed script to flash a given binary saved at a known location

11 REPLIES 11
Andrew Neil
Super User

Would the CubeProgrammer command-line version be OK?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
GHM
Associate II

Thanks for the reply. We need a bat file or script to flash a binary to stm32h503rbt6 using st link ie jtag or RS232

MOBEJ
ST Employee

Hello @GHM , 


I recommend checking the STM32Cube command-line toolset quick start guide, specifically UM3088 on page 4. It provides helpful information on using the STM32CubeProgrammer as a command-line tool. This should guide you through the necessary steps and commands.

BR

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

you can follow a bat file used to flash Demo binary for STM32H747I-DK boards , download the demo package in ST.com from this link : https://www.st.com/resource/en/compiled_demos/stm32h747i-disco_demo.zip  ,

After downloading, navigate to the following path within the package: stm32h747i-disco_demo.zip\STM32H747I-DISCO_demo\Binary. There, you will find the program_hexfile.bat file, which is specifically designed for the STM32H747I-DK Demo binary. Reviewing this batch file can assist you with your specific case.

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LCE
Principal II

The STLINK-V3SET offers a windows drive, if you connect it to your destination board, you can use a simple windows batch file to copy to this drive, the ST-Link then writes it to the destination STM32.

So it's basically only this in the *.bat file in the project folder, if "F:" is the ST-Link drive:

copy Release\STM32H733_work.bin F:

GHM
Associate II

Thanks all. However, neither of the solution is loading the binary to the MCU. Request for a dedicated bat file/script to load the binary to STM32H503RBT6

So show what you've tried.

Are you getting any error messages?

You need to give full details:  we don't have crystal balls to see what's going on in your setup - or even what your setup is!

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
GHM
Associate II

1) Added the below jlink & bat to the source folder & then ran the bat file but no flashing happened

jlink file-"C:\Program Files (x86)\STMicroelectronics\stlink_server\stlinkserver.exe" STM32h503RBT6 -if SWD -speed 4000 -autoconnect 1 -CommanderScript C:\SSB\Develop\SSB_ALPHA\SSB_ALPHA\Debug\flashonly.jlink

flashonly.bat-"C:\Program Files (x86)\STMicroelectronics\stlink_server\stlinkserver.exe" STM32h503RBT6 -if SWD -speed 4000 -autoconnect 1 -CommanderScript C:\SSB\Develop\SSB_ALPHA\SSB_ALPHA\Debug\flashonly.jlink

2) Other .bat files containing the bin files in the same folders

a)

@Echo off
REM Change these paths according to your setup

SET BINARY_FILE=SSB_1.bin
SET CUBE_PROG_PATH="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
SET STLINK_SN= REM (Optional: specify ST-LINK serial number if needed)

REM Set address for STM32H503RB6 (usually 0x08000000 for main flash)
SET FLASH_ADDR=0x08000000

REM Go to CubeProgrammer directory
cd /d %C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin%

REM Flash binary using STM32CubeProgrammer CLI
STM32_Programmer_CLI.exe ^
-c port=SWD 40000
-d %~dp0%BINARY_FILE% %FLASH_ADDR% ^
-rst

b)

:: STM32CubeProgrammer Utility flash script

@Echo OFF
@setlocal
::COLOR 0B

:: Current Directory
@SET CUR_DIR=%CD%

:: Chip Name
@SET CHIP_NAME=STM32H503RBT6
:: Main Board
@SET MAIN_BOARD=-DISCO
:: Demo Name
@SET DEMO_NAME=STM32Cube_Demo
:: Demo Version
@SET DEMO_VER=V1.0.0
:: Hex filename
@SET HEX_FILE="%SSB_1%.hex"
@IF NOT EXIST "%HEX_FILE%" @SET HEX_FILE=%SSB_1%.hex"
@IF NOT EXIST "%HEX_FILE%" @Echo %HEX_FILE% Does not exist !! && GOTO goError

:: Board ID
@SET BOARD_ID=0
:: External Loader Name
@SET EXT_LOADER=MT25TL01G_%CHIP_NAME%%MAIN_BOARD%

@SET STM32_PROGRAMMER_PATH="%Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
@IF NOT EXIST %STM32_PROGRAMMER_PATH% @SET STM32_PROGRAMMER_PATH="%ProgramW6432%\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
@IF NOT EXIST %STM32_PROGRAMMER_PATH% @SET STM32_PROGRAMMER_PATH="%ProgramFiles%\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"
@IF NOT EXIST %STM32_PROGRAMMER_PATH% @Echo STM32CubeProgrammer is not installed !! && GOTO goError
@IF NOT EXIST %STM32_PROGRAMMER_PATH% @Echo %STM32_PROGRAMMER_PATH% Does not exist !! && GOTO goError
@SET STM32_EXT_FLASH_LOADER=%C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\api\lib\ExternalLoader%.stldr
@IF NOT EXIST %STM32_EXT_FLASH_LOADER% @Echo %STM32_EXT_FLASH_LOADER% Does not exist !! && GOTO goError

@SET STM32_EXT_FLASH_LOADER=%C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\api\lib\ExternalLoader%.stldr

TITLE STM32CubeProgrammer Utility for %CHIP_NAME%%MAIN_BOARD%

:: Add STM32CubeProgrammer to the PATH
@SET PATH=%STM32_PROGRAMMER_PATH%;%PATH%

@Echo.
@Echo =================================================
@Echo Erase and Flash all memories and reboot the board
@Echo =================================================
@Echo.
STM32_Programmer_CLI.exe -c port=SWD index=%BOARD_ID% reset=HWrst -el %STM32_EXT_FLASH_LOADER% -e all -d %HEX_FILE% -HardRst
@IF NOT ERRORLEVEL 0 (
@GOTO goError
)

@GOTO goOut

:goError
@SET RETERROR=%ERRORLEVEL%
@COLOR 0C
@Echo.
@Echo Failure Reason Given is %RETERROR%
@PAUSE
@COLOR 07
@EXIT /b %RETERROR%

:goOut

 

Again, do you get any errors messages with that?

Before going to a .bat file, have you got it working by typing manually?

 


@GHM wrote:

cd /d %C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin%


That doesn't look right: the %...% should enclose a symbol name for expansion.

Did you mean:

cd /d "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin"

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.