Audio Sample Rate Conversion Libs: Specs?
Heyho,where can I find the specs for STM32 Audio Sample Rate Conversion libraries ?I mean some hard specs like SNR & THD, as can be found in any hardware SRC datasheet.Merci!
Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.
Heyho,where can I find the specs for STM32 Audio Sample Rate Conversion libraries ?I mean some hard specs like SNR & THD, as can be found in any hardware SRC datasheet.Merci!
Hi,I’m using an STM32L412RB where the USB DM/DP lines are already configured as a Virtual COM Port (USB CDC device).Now I want to communicate with an RS485 bus without changing the existing board hardware.My idea is to build a small adapter board tha...
I have selected the STM32H743ZIT6 MCU for our project. Our application requires storing 22-byte data for approximately 1.5 lakh entries in RAM. Based on our calculations, we need an external memory of at least 4 MB to 8 MB. The previously considered ...
I want to initialize and drive 24 bits LCD display with the driver ST7282. I did not find any driver file online. Can someone please suggest me the similar driver that I can use to drive the display????
Hi,need information about the soldering profile for LQFP100 pin package in case, soldering the IC manually with temperature controlled soldering station
dear all!i'm trying to set up model run external with matlab via TCP/IP. when i build it have some issue, i don't how to config. i build model on Matlab 2024b and STM32CubeMX 6.4. can you share me how to set up step by step.
Hello!I'm using STM32F401 (Blackpill board).I made an experiment like this. I set my PC serial setup as 8n1 and UART6 serial setup as 8n2.And started communication between my PC and UART6.It was okay. Nothing went wrong. For both sides, tx and rx.Bef...
Hi,has anybody already implemented the LAN9253 via SPI?I´m trying since several month to implement the Software framework - without success...EtherCAT Software Framework User's Guide (microchip.com) Best regards, Achim
Hi thereI am working on a custom board with a s2-lp radio on it. The only difference to the STM generate s2-lp SubGhz project is that I use PA5 for radio_sck (see attached Project). After playing a while with my I-NUCLEO-S2868A2 shields suddenly the ...
In this Getting Started Tutorial video we are going to dive into generating an audio I2S stream. We will be creating dual SINE waves (Left/Right) at 96 kHz sample rate. #STM32 #Tutorial #GettingStarted #STM32CubeIDE #STM32CubeMX #I2S #DMA #STM32World...