cancel
Showing results for 
Search instead for 
Did you mean: 

Technical issues related to RF transistor SD2933

H_YM
Associate II

We want to use this transistor to drive piezoelectric ceramics at 900KHz, 1.7MHz, and 3MHz, which requires about 50W of power.

I have the following questions and need help:

1. Can this transistor be used at a frequency of 900kHz? Can it only be used in frequency bands above 1MHz?

2. The data sheet provides a test circuit under 30MHz conditions. We do not fully understand the functions and principles of the FB2 and T2 components. Can you explain it to us? We guess that the function of this component should be for impedance conversion. Can the FB2 and T2 components be replaced with a simple and easy-to-understand transformer impedance conversion form (FT-43 core) like the previous stage?

3. We want to imitate the 30MHz test circuit and apply it directly to the production environment. Are there any other issues worth noting during this process?

1 REPLY 1
SofLit
ST Employee

Hello and welcome to this community.

Please kindly write in English to let other members help you efficiently.

Thank you.

 

Translation:

Subject: Technical issues related to RF transistor SD2933:We want to use this transistor to drive piezoelectric ceramics at 900KHz, 1.7MHz, and 3MHz, which requires about 50W of power.

I have the following questions and need help:

1. Can this transistor be used at a frequency of 900kHz? Can it only be used in frequency bands above 1MHz?

2. The data sheet provides a test circuit under 30MHz conditions. We do not fully understand the functions and principles of the FB2 and T2 components. Can you explain it to us? We guess that the function of this component should be for impedance conversion. Can the FB2 and T2 components be replaced with a simple and easy-to-understand transformer impedance conversion form (FT-43 core) like the previous stage?

3. We want to imitate the 30MHz test circuit and apply it directly to the production environment. Are there any other issues worth noting during this process?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.