cancel
Showing results for 
Search instead for 
Did you mean: 

STM32IDE(1.18.0) error fails to start GDB after download

安和486mmk
Associate

Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).

STM32IDE (1.18.0) for the STM32F103C8T6 always fails to start the GDB after download and installation, and there is no method on the web page or official manual. Recent successes are STM32IDE (1.17.0) still working in mid to early February, and STM32IDE (1.17.0) not working at the end of February. (ST-link V2 to STM32F103C8T6)

Original:

3C8T6M32F的STM32IDE (1.18.0) 下载安装后总是无法启动 GDB,网页上的方法和官方手册也没有。最近的成功是 STM32IDE (1.17.0) 在 2 月中旬到初仍在工作,而 STM32IDE (1.17.0) 在 2 月底无法正常工作。(ST-link V2 to STM32F103C8T6)屏幕截图 2025-03-14 201237.png

12 REPLIES 12

Are you sure that it actually works out cheaper than buying a Nucleo board - which includes a genuine ST-Link?

A Nucleo-103 is under £10 !

AndrewNeil_0-1742226419901.png

 

So long as you're aware that you are using fake/clone gear - and the many difficulties that may cause.

Again, see this thread for the grief the fakes can cause ...

And, of course, you can't count on support from ST!

Are you sure you have that wiring correct?

AndrewNeil_0-1742226827074.png

AndrewNeil_1-1742226887940.png

 

 

swd -- swc  puzzled . :D

If you feel a post has answered your question, please click "Accept as Solution".