cancel
Showing results for 
Search instead for 
Did you mean: 

STM32IDE(1.18.0) error fails to start GDB after download

安和486mmk
Associate

Edit by ST Moderator: This post has been translated from Chinese to comply with the ST Community Terms and Conditions (§10.2).

STM32IDE (1.18.0) for the STM32F103C8T6 always fails to start the GDB after download and installation, and there is no method on the web page or official manual. Recent successes are STM32IDE (1.17.0) still working in mid to early February, and STM32IDE (1.17.0) not working at the end of February. (ST-link V2 to STM32F103C8T6)

Original:

3C8T6M32F的STM32IDE (1.18.0) 下载安装后总是无法启动 GDB,网页上的方法和官方手册也没有。最近的成功是 STM32IDE (1.17.0) 在 2 月中旬到初仍在工作,而 STM32IDE (1.17.0) 在 2 月底无法正常工作。(ST-link V2 to STM32F103C8T6)屏幕截图 2025-03-14 201237.png

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @安和486mmk to the community!

please upload a legible photo (front and back) of the ST-LINK/V2.

The board with STM32F103C8T6 - is it a so called Blue Pill?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

12 REPLIES 12
Peter BENSCH
ST Employee

Welcome @安和486mmk to the community!

please upload a legible photo (front and back) of the ST-LINK/V2.

The board with STM32F103C8T6 - is it a so called Blue Pill?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Chief III

See message in console : wants st-link update first !

So go menu Help -> st-link upgrade ...

then try again connect/debug .

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Guru

It says you need to upgrade the STLink firmware. I would suggest starting there.

If you feel a post has answered your question, please click "Accept as Solution".

但我已经更新了它


Google Translate:

But I have updated it

1000018363.jpg

1000018364.jpg

  

Fake board, fake programmer. What could go wrong?

If you feel a post has answered your question, please click "Accept as Solution".

1. did you upgrade ?

See message in console : wants st-link update first !

So go in IDE : menu Help -> st-link upgrade ...

success ? 

2. connect setting in IDE: software reset

 -> then try again connect/debug .

-> then it should work.

If you feel a post has answered your question, please click "Accept as Solution".

没有推荐的便宜的STlink,官网太贵买不起了。


Google Translate:

I don’t have any recommended cheap STlink products. The ones on the official website are too expensive and I can’t afford them.