2020-07-23 5:38 AM
Hi
Thank you for reply
I have three ST10F276 Boards in that One is completely not detected,second one detected once after that not detected, third one continuously detecting ,
For your information All same boards
please suggest Why I am getting this problem.
And in one detected board I selected all banks and erased once is it disturb the bootstrap method?(in image I selected all bank and erased once)
Thanks & Regards
Eshwar
2020-07-28 2:40 AM
Hello,
There is certainly some differences between your boards as you have different behaviors.
I suspect a hardware problem on the failing board : bad soldering or damaged component.
I suggest to start with the basics:
check all the supply pins first then the oscillator, reset and RPD pin.
V18 is the output of the regulator and should have 1.8V .
Debugging should be easier as you have a working board in your hands.
2020-07-28 9:33 PM
Hi Max
here we are getting V18 voltage 0v, and RPD pin Voltage 0.2V ( In Working Boards 5V)
Please tell me Is ST Controllere Damaged?
Any we ordered New Controlleres.
Regards
Eshwar P