Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC Clock 'hello world' program STM8L cpu

Posted on June 30, 2013 at 13:07Can anyone help with some code to use the RTC clock as a clock. I'm using the STM8L-Discovery board and not sure how to set the chips registers and to set / read time to the LCD display. I just need a 'hello world' pr...

Active/Halt wakeup with RTC

Posted on May 03, 2013 at 14:36Hi ,I am a new user of STM8.  In my project I am using Active/halt mode an it wakes up with RTC Wakeup operation. My problem is, it is always waking up same times. it's equal to 3ms. I want update auto wake up times. I...

Routing Interface (RI)

Posted on May 07, 2013 at 14:58I am using the STM8L151C6T6. I would like to route PD6 to TIM1 Input Capture IC2. The following code executes but does not change the RI_ICR1 register value and the routing does not take place either.     GPIO_Init(POR...

wynand by Associate II
  • 1078 Views
  • 1 replies
  • 0 kudos

COSMIC LKF File

Posted on May 27, 2013 at 11:48Hi All, I want to execute some command in .lkf file for COSMIC Compiler condionally. is it possible?? Pseudo code is as below: /*--------------------------*/ #ifdef TRUE obj\libisl.sm8 #else obj\libis0.sm8 #endif /*---...

Storing some calibration data in FLASH memory

Posted on April 17, 2013 at 22:35Hello, I'm looking into storing some calibration data for my application into FLASH memory since my EEPROM space is very valuable and I cannot spare any of it. The cal data would only be written once (upon the first ...

use rs232 uart with stm8l discovery board

Posted on August 12, 2011 at 01:06Hi, I would like to use the uart device of the stm8l chip on the stm8l discovery board. I notice that uart and cristal are shared on the same pins (PA2 and PA3) Do you think it is possible to use the uart when the s...

pub by Associate
  • 872 Views
  • 1 replies
  • 0 kudos