Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM8L152C6] SPI SCK low signal

Posted on November 07, 2013 at 15:42Hi everyone,I'm new to the STM community and those microcontrollers too, I'm learning to use them;)I've configured a communication based on SPI through DMA, everything is working excepting the SCK. I've configured...

0690X00000604zqQAA.png

STM8S003 MCU and emulator question

Posted on November 07, 2013 at 12:40We use the STM8S003 MCU in one of our products and specifically we use the LINbus communications in slave mode. In the 003 datasheet it says the UART (UART type 1) can actually only support LINbus master mode. Whe...

alex2 by Associate
  • 891 Views
  • 0 replies
  • 0 kudos

HSI Power Down

Posted on June 10, 2013 at 16:48Hello everybody,I'm programming a STM8L152C6 on the STM8L-discovery. Wanting to improve the consomption I tri to power down the HSI. For that I use the instruction  // Clock source   CLK_LSICmd(ENABLE);   CLK_SYSCLKSo...

quentin by Associate
  • 1255 Views
  • 2 replies
  • 0 kudos

IWDG & WWDG for stm8l151c6 halt active mode

Posted on June 13, 2013 at 13:27I want to use stm8L watch dog in halt/halt-active mode. my system wakes up by RTC.1. when I choice Independent watchdog, a watchdog reset happens when system is in halt/halt-active mode. As you know, the option byte(0...

_checksum16()

Posted on October 09, 2013 at 23:02I'm using Cosmic 4.3.6 compiler & have a project with greater then 32k code.  I need to checksum the flash at startup and periodically during runtime to satisfy UL60730.  My first project (about 12k code size) went...

jdf25252 by Associate II
  • 2284 Views
  • 3 replies
  • 0 kudos

start and stop the tim1 -> adc -> dma chain

Posted on October 25, 2013 at 00:18I have an STM8L application that needs to scan several ADC channels on a fixed time basis, so I used the ADC_DMA code from the STM8L standard peripheral examples as a starting point. The timer is set to a 1KHz trig...

mark23 by Associate
  • 786 Views
  • 0 replies
  • 0 kudos

<< shift easy question

Posted on October 10, 2013 at 08:52Hello, I have a simple question: uint32_t temp; temp |=  ((uint32_t)1 << 16); without retyping it does not work (although if I add the expression to Watch, it shows expected 1 on 16th bit of temp). Why? I use Cosmi...

pok-on by Associate II
  • 1655 Views
  • 3 replies
  • 0 kudos

VREFINT_FACTORY_CONV

Posted on September 11, 2013 at 14:17Hello,I am currently working on STM8L15C6. For my application I need to read the value stored at location VREFINT_FACTORY_CONV. The value at this memory location is 0xFF. We were assuming the value to be somewher...

megha by Associate
  • 1430 Views
  • 3 replies
  • 0 kudos