Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

gdi-error [40201]

Posted on March 20, 2015 at 18:08hello i started up a new pc wirh windows 7 proffesional  can install the toolset for the stm8s but when i try to debug it gives me that error  ''gdi-error [40201] gdi-error [40201] but when i try the programmer and j...

eDesign suite not working

Posted on March 13, 2015 at 11:18Whenever I try to start a Project using the a VIPERxxx non-isonalted AC/DC buck converter I get the following error message: HTTP Status 404 - /analogsimulator/flex_app/bin/assets/config/smps_app_acdc_design.htmlWhen...

Blink all elements on LCD

Posted on March 13, 2015 at 17:42 Hey, I want a very simple example: All elements on LCD should blink at startup(so in this very simple example: for everytime ;) So I want to use the BlinkConfig Function from the StdLibrary... My e...

flol2204 by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

Clock x ports doubts

Posted on November 19, 2014 at 12:13Helloi�m new in STM8s105 microcontroller and cosmic c compiler.i wrote a small program:i set the clock with internall clock with prescaler 8:CLK_CKDIVR= 0b00011000;it means that my uc will operate at 2 MHz, right?...

STM8S Discovery - blink led1

Posted on March 09, 2015 at 19:16 Hi guys, I am trying to understand the ports of stm8s105c6.. I want to blink the led1 of the board on port PD0.. For what I understand I need to configure PD0 as Output, and after, drive curr...

lmx1 by Associate II
  • 862 Views
  • 0 replies
  • 0 kudos

STM8L Discovery Board SWIM Out

Posted on January 04, 2014 at 15:58Hello,I would like to know that if the SWIM output on the STM8L discovery board can be used to program/debug other STM8/STM32 Boards? instead of the STM8L chip on the same PCB.Thanks

gada by Associate III
  • 814 Views
  • 2 replies
  • 0 kudos

STHV748 high supply current

Posted on February 20, 2015 at 11:18Hello Community, I want to use the STHV748 for pulsing film-Arrays. The circuit is build like the reference circuit in the Application Note AN3961 figure 33.  The input line are low  so that the output from the ST...

0690X00000605anQAA.png