Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

using stvp_cmdline to program st7flites5

Posted on November 03, 2014 at 03:35Hi all, I encountered few issues when using STVP to program a ST7Flites5.  Can anyone advice me on possible solutions?  Tks in advance. 1.    STVP does not provide a erase before programming option for ST7Flites5....

benedict by Associate II
  • 1932 Views
  • 2 replies
  • 0 kudos

UART expample

Posted on June 14, 2015 at 22:39Hi !Until now I used mostly arduino procesors, and recenzly got one discovery board.I'm very new in programming for STM8 processors. I had searched site for expample project for UART communication, but I can't find so...

mladen by Associate II
  • 1353 Views
  • 1 replies
  • 0 kudos

Reprogramming STM8S005K6

Posted on June 14, 2015 at 22:10Good evening ST Community, I am a complete newbie in microcontrollers and programming. Only advanced in Excel macro building, but not sure if that will help =D Well, also had some time spent on Arduino a few years ago...

sattarov by Associate
  • 848 Views
  • 0 replies
  • 0 kudos

sdcc 3.5.0 rc1

Posted on June 11, 2015 at 18:18sdcc 3.5.0 is to be released soon. There already is release candidate 1. You can download the release candidate and have a look at it. The more eyes on it, the less likely are hidden bugs. The main changes from previo...

COSMIC LICENSE error

Posted on June 13, 2015 at 18:18I have got cosmic license file and copied it to ''license'' sub-directory of the compiler. But while compling getting error as  FlexLM System clock has been set back. I contacted to cosmic they replied as This messag...

jagspaul by Associate II
  • 1842 Views
  • 2 replies
  • 0 kudos

openocd

Posted on May 22, 2015 at 18:19Hello,I try to integrate a STM8 into an existing projects build system. I need basic support to flash a controller and ideally some basic debugging support. I've managed to do this for a STM32 controller with openocd. ...

torsten2 by Associate II
  • 1241 Views
  • 2 replies
  • 0 kudos

Dubts, how to reset stm8s

Posted on December 01, 2013 at 08:05Hi guys, I am new to STM8s discovery... I have done the following code: stm8/     ;mapping.asm exists ...     segment 'rom'      start     bset $5011,#0;sets PD0 to input loop_main     ldw X,#$FFFF loop_delay    ...

lmx1 by Associate II
  • 1633 Views
  • 3 replies
  • 0 kudos

Reading data from array

Posted on May 29, 2015 at 00:03Hi, I'm developing application which include I2C communication, so I have implemented code from AN8231. So far it works fine and I got data from I2C peripheral in input_buf[]. Data are valid, and I can see them in watc...

delkons by Associate
  • 918 Views
  • 1 replies
  • 0 kudos

PWM Input measurement - TIM1

Posted on May 29, 2015 at 15:14Hello all,I want to use TIM1 and its PWM input mode to obtain duty cycle and frequency of measured signal on STM8S003. But I have uncertainty about measured value.Snippets of codevoid initialization () {//System Clocks...