Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading SPI port - first byte?

Posted on April 08, 2014 at 16:53Maybe some of you with SPI experience can spot this one easily. I have a SPI slave device connected to my STM8L152. I watch the clock and data stream to the device requesting a read of a register, and then I can see ...

vince by Associate III
  • 1485 Views
  • 1 replies
  • 0 kudos

why is my interrupt not working???

Posted on September 10, 2015 at 07:26 hello, I've been trying to blink an led using an overflow interrupt with timer 4 on the sm8l discovery board. So far I haven't made it work. I'm currently using IAR Embedded Workbench with the Std lib...

Difficulties in finding the ideal transformer

Posted on August 17, 2015 at 21:48My first project using the tool eDesignSuite and I'm developing a switching power supply with a 85VAC to 265VAC input voltage with 24VDC output and 5A of output current. My difficulty is in finding the transformer t...

vinicius by Associate
  • 1775 Views
  • 5 replies
  • 0 kudos

STM8S003 - SPI Receive

Posted on August 30, 2015 at 01:49 I'm at my wit's end, I cant seem to make SPI receive work properly. This is a cut from the S003 reference manual: This is the capture from the logic analyzer: And this is th...

0690X000006051mQAA.png 0690X00000604qzQAA.png
bjerman by Associate II
  • 731 Views
  • 0 replies
  • 0 kudos