Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where are the STM8S Firmware Libraries?

Posted on September 11, 2015 at 18:53ST's documentation keeps mentioning the STM8S firmware libraries, but no document number is listed. I've been searching ST's site for some time, but no results returned. Maybe they've been renamed?Any info or sug...

ih55t by Associate
  • 1443 Views
  • 3 replies
  • 0 kudos

Error in complier stage

Posted on September 09, 2014 at 15:19Dear sir,    I am starting to study STM8S and build a simple code. But after complier, it show '' &sharperror cpstm8 stm8s103.h:600(0+6) missing ; main.c:  The command: ''cxstm8 +debug -pxp -no -l +mods0 -pp -i''...

How to use the UART on the STM8A-DISCOVERY?

Posted on December 25, 2015 at 21:38I want to use the UART on the STM8A-DISCOVERY boards. However, AFAIK, the STM8A RX and TX pins are not connected to any header on the boards. There are open solder bridges connecting them to the ST-Link/v2 interfa...

tim4 not work with STM8S103K3

Posted on January 07, 2016 at 16:04Hello:I'm write code from STM8S105C4T6 using tim4 basic timer, the code is store  in INTERRUPT_HANDLER routine, anythings work.I'm change to use  STM8S103K3T6C (smallest) , the interrupt routine don't fire,I change...

ekpol by Associate II
  • 1547 Views
  • 2 replies
  • 0 kudos

STM8S SelfTest

Posted on January 07, 2016 at 14:46The original post was too long to process during our migration. Please click on the attachment to read the original post.

silvio2 by Associate
  • 715 Views
  • 0 replies
  • 0 kudos