STHV800 single polarity HV
Posted on February 18, 2016 at 10:16Can I use only one HV power source (HVM or HVP)? I need pulses single polarity. #sthv800-single-polarity-hv
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Posted on February 18, 2016 at 10:16Can I use only one HV power source (HVM or HVP)? I need pulses single polarity. #sthv800-single-polarity-hv
Posted on February 26, 2016 at 10:04We are using assembler code in our C-code. The jp instruction is used to jump into the booloader. But sporadic the jp instruction is not working. We have also used jpf instruction. Without success. What can be the...
Posted on February 26, 2016 at 03:21Hi,I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperr...
Posted on February 25, 2016 at 13:10I below code, I am reading ADC counts and sending it over CAN. ADC is working properly for _SINGLE conversion mode.... But it is not working for CONTINUOUS Conversion mode mode.
Posted on February 23, 2016 at 12:22 We are using the LIN Driver suit V 5.1.0 from ST microelectronics. The demo project provided in that is having a lin_basic_demo.ldf and lin_basic_demo.lgn files. I was successfully able to regenerate lin_cfg.c, l...
Posted on December 10, 2015 at 14:06The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on February 17, 2016 at 18:49I'm trying to design a constant current driver in eDesign Studio using the ST1CC40DR chip. I've set my output requirements to 4.8V and 1.2A and the input is 12V DC. With a 2% LED ripple current and 10% inductor ri...
Posted on February 18, 2016 at 05:02Hi,I'm using DMA to transfer the data from USART1,The length of the data is varible.So I open the USART IDLE LINE interrupt.I try to set the DMA data counter to zero by using the function ''DMA_SetCurrDataCounter(...
Posted on February 15, 2016 at 14:37Hi all: I can't find out what the difference is between those 2 micro, May by someone will help :) Thanks a lot! Regards Per
Posted on February 12, 2016 at 14:20Hello,I want to use I2C Communication between two stm8s208cb MCUs. I use stm8s standard peripharel library. My code:Master:&sharpinclude ''stm8s.h''&sharpdefine I2C_SPEED 300000&sharpdefine OWN_ADDRESS 0xA0 ...