Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S Timer1 input capture issue

Posted on May 17, 2016 at 17:30Hello am working with the timer1 input capture of an STM8S103F3. No input is registered by the input capture module though I fed it with square waves from 10Hz all the way up to 1MHz. The same square wave registers pro...

jf by Associate
  • 846 Views
  • 0 replies
  • 0 kudos

Hello World

Posted on April 19, 2016 at 03:16Hello everybody. Can someone point me to a simple ''Hello world'' LED blinking example for STM8?My situation is as following:I found http://www.electroons.com/blog/stm8-tutorials-2-hello-world-program/ and I tried to...

d_aliaga by Associate II
  • 1559 Views
  • 2 replies
  • 0 kudos

STM8S207SB checksum fails with cosmic compiler

Posted on April 18, 2016 at 14:20Hi!I just tried to verify the FLASH according to CLASS B considerations. I followed the manual by using -ck for .text and -ik (.checksum area) flags for the linker,The descriptor is inside the s19 file, the map file ...

hjs by Associate II
  • 2330 Views
  • 3 replies
  • 0 kudos

VIPER 06L for 3.3VDC

Posted on April 13, 2016 at 19:13Hi, I am using the eDesign Suite to make a 3.3VDC Power Supply , but I am facing some problems .First of all , I got the schematic from the eDesign Suite and make it on Breadboard , It should has an output of 3.3VDC ...

0690X00000605dHQAQ.png

Source code for STEVAL-IAS003V1

Posted on April 19, 2016 at 07:45Hello,I amlooking for source code of ST STEVAL-IAS003V1 evaluation board board.UnfortunatelyI can not find in on ST web site and trough the Google to...Pleasehelp.Regards,Alex.

STM8 firmware library

Posted on April 14, 2016 at 09:32HelloI have been reading a document called Getting Started with the STM8 and they mentioned the ''STM8 firmware library''However I have spent a lot of time (really too much) trying to find this library. Searches insi...

d_aliaga by Associate II
  • 2691 Views
  • 4 replies
  • 0 kudos

ST7268x Production Tool

Posted on April 13, 2016 at 14:45Hi all , i need to re-configure  an old ST72681 fast usb flash controller . The problem is that i cannot find the tool needed to configure it . Does anybody know where this tool can be found ? Thanks in advance . L...

Big problem with STVD

Posted on April 05, 2016 at 12:15I have a workspace containing several projects; one of those projects has several building configurations. Randomly, the STVD switches the settings between the varoius configurations in this project, this way I am ne...

i2399 by Associate III
  • 1247 Views
  • 1 replies
  • 0 kudos

Where to find how i read analog values?

Posted on April 09, 2016 at 18:07Hello,it frustrates me that i don't find the information i need to read an analog value from a temperature sensor. I only have the overall documentation file, which's ADC-part is 1/4 page, and a documentation dedicat...

loder by Associate II
  • 842 Views
  • 0 replies
  • 0 kudos