Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Build Error using STVD.

Posted on November 29, 2017 at 19:18I'm new to STVD, but I've used two other microcontroller IDEs in the past.  I have a standard Windows 10 machine with the standard STVD installed.  This is a simple test using Assembler code and the STM8S003F3P mi...

Zero Cross Detection on STM8L151K4T6

Posted on February 25, 2018 at 20:15Hi,I want to detect zero crossing of AC mains by using stm8l151kxxx. In referance manual it says there are two comparators for zero cross detection but it doesn't give detailed information about hardware implement...

stm8_uart1.c error

Posted on October 16, 2013 at 10:36Hello, I am not sure if this is a proper place for reporting errors. If not so, please tell me, where to report it. The error is in stm8_uart1.c module of STM8S_StdPeriph_Lib_V2.1.0. According to description of UAR...

pok-on by Associate II
  • 1375 Views
  • 1 replies
  • 0 kudos

how i choise transformer?

Posted on February 16, 2018 at 20:18hi my name is mehdi . I'm using eDesignSuite for a Viper 27LN. how i choise transformer  with Transformer Specifications?Transformer Specifications:    fsw: 60 kHz - Isat ≥ 757 mA - Lp: 2.06 mH ± 10 % - leakage...

STVD start debugging shortcut

Posted on February 18, 2018 at 21:45Hello,In ST Visual Develop there is no shortcuts for 'Start debugging' and 'Stop debugging'.Why it wasn't implemented yet?These shortcuts are standard in many others IDE.Can it be configure in seetings or external...

Resolved! What does sim() function do

Posted on February 16, 2018 at 11:38I am trying to understand what 'sim()' does in the example code that comes on the STM8L-DISCOVERY eval board (Introduction to STM8L15x power saving modes using the STM8L-DISCOVERY IDD measurement feature) where th...