Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L052R8 NRST ESD PROBLEM

Posted on April 25, 2018 at 03:39Hello..I am using a circuit board using the STM8L052R8.This board generates the voltage to be applied to MCU after applying 4.8VDC voltage by using 3.3VDC regulator.IWDG and BOR are used in the firmware.However, when...

Interrupt that will not expected

Posted on April 23, 2018 at 03:59Hello,- MCU : STM8L101K3I am using Port A.2 for interrupt and Port D.2 for general gpio.GPIO_Init(GPIOA,GPIO_Pin_2, GPIO_Mode_In_FL_IT); EXTI_SetPinSensitivity(EXTI_Pin_2, EXTI_Trigger_Falling); GPIO_Init(GPIOD, GPIO...

0690X0000060AjPQAU.png

STM8 Vcap voltage

Posted on April 21, 2018 at 07:31Hi everybodyI have designed my own pcb stm8 based on discovery board stm8AF52 5v power I can program it easily without any problem but Vcap voltage is 2.4 instead 1.8 what is the problem here?thanks for your help in ...

Yas Yasin by Associate II
  • 1276 Views
  • 1 replies
  • 0 kudos

What is the reliability of the RTC?

Posted on April 21, 2018 at 14:35Hello everyone,Very much I ask to respond who knows. Whether methods are applied of providing increased reliability of real-time timers, for example redundant coding or majority calculations. And what are the values ...

www.colecovision.eu

Posted on February 11, 2018 at 20:04Another comparison of C compilers for the STM8 About two years ago, I did a comparison of C compilers for the STM8. It can now be found at http://www.colecovision.eu/stm8/compilers-2016.shtml.I also redid the comp...

STM8L1526-eval board problem

Posted on April 19, 2018 at 14:52Hello, i have an STM8L1526 board, and i don't success to connect with my computer. I use ST visual develop but it doesn't work. I want to use the STM8L152C6 to drive some of led on extern electronic plateform ( proto...

STM8AF6266 to control LED wiping sequence

Posted on April 19, 2018 at 02:55I am trying to use STM8AF6266 to control the LED wiping sequence.PC1~PC7 connect to 7 branches of LEDs.By programming the flash, I was able to observe one-time wiping sequence, but I would like to see continuous wipi...