Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to count PWM Pulse coming on GPIO?

Hi, I am a newbie in writing code on MCU's.I am using STM8S003K3 with which several fan controllers are attached on different GPIO. I need to count PWM pulse whenever it comes on any port and then identify the pin no of that port. How to count pulse ...

RPriy by Associate II
  • 723 Views
  • 0 replies
  • 0 kudos

stm8l lcd setting

HOW to code this table?void LCD_GLASS_Init(void) { /* The LCD is configured as follow: - clock source = LSE (32.768 KHz) - Voltage source = Internal - Prescaler = 2 - Divider = 18 (16 + 2) - Mode = 1/8 Duty, 1/4 Bias ...

0690X000009Z7tfQAC.png

Resolved! STM8 HSE

Hi,I am testing an application, and currently is working properly with HSI configured to 16MHz.Now I want to enable the HSE.I am using a NUCLEO-8S208RB. I have soldered an external crystal on X2, and i have configured the board with 12pF capacitors a...

ACogl by Associate III
  • 1789 Views
  • 1 replies
  • 0 kudos

M24C02-DRMF3 EEPROM: Package Marking

Hi ST,We are implementing an M24C02-DRMF3 EEPROM based design and wanted to confirm the correct package marking for this device including part number, die version, date code and fab facility. Although the Data Sheet includes the WFDFPN8 mechanical in...

CCamp by Associate
  • 1519 Views
  • 2 replies
  • 0 kudos

Resolved! Is a Mosfet P382 ?

Hi, I'm looking for what I think is a Mosfet with this print, see the attached picture.I need to replace it because it's burned, but I don't know the features.Anyone can help me about ?Thanks a lotIvano

IGiac by Associate
  • 1997 Views
  • 2 replies
  • 0 kudos

STVD workspace location limitation?

I wish to use STVD to set up a new workspace on a mapped common drive but it whereas I can see and go to a mapped drive with the Atmel IDE etc the STVD IDE doesnt appear to recognise it. Is this a known limitation or something I am doing wrong?

BCowa by Associate II
  • 806 Views
  • 0 replies
  • 0 kudos