Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is the part M95M02-DWMN3TP/K is SEE tested? If so, what is the SEE rate or SEU cross section What is the process technology of this part? What is SEL rate?

I am currently working on SEE analysis for our product which uses the above stated part. SO I need the following info:Is the part M95M02-DWMN3TP/K is SEE tested? If so,what is the SEE rate or SEU cross sectionWhat is the process technology of this pa...

BUG: HSE_Value should be HSE_VALUE in stm8s.h

This bug is several years old and should really be fixed.In stm8s.h, the following line ...#if !defined HSE_Value... should (obviously!) be ...#if !defined HSE_VALUE... in order to allow HSE_VALUE to be defined on the command-line.I just found out th...

pacman by Associate III
  • 2899 Views
  • 4 replies
  • 0 kudos

STVD not handling EEPROM data correctly

I have an issue when I am using STVD with Cosmic to write a value to EEPROM and read it back.Example code :/* MAIN.C file *  * Copyright (c) 2002-2005 STMicroelectronics */#include "stm8s.h"#include "stm8s_flash.h"@eeprom unsigned char eeValue;unsign...

BCowa by Associate II
  • 1573 Views
  • 2 replies
  • 0 kudos

STVP_CmdLine file read

Posted on May 22, 2015 at 16:31Hi folks I'm trying to read the (unprotected) contents of the data flash of an STM8L processor via the command line application provided. As this works in the GUI version I assumed I should be able to specify a file to...

jro by Associate III
  • 2612 Views
  • 3 replies
  • 2 kudos