Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I would like some doubts clarified

I've been working with STM8S chips for about 2-3 months now, and would like my doubts clarified:What is the state of the RAM in the chip after a software/watchdog reset(Not BOR or POR, obviously). I have assumed the RAM is not disturbed by the Reset,...

I have stm8l discovery and Can any one help with i2c configuration here. I am using LP55231 led driver and I do not know whether this configuration is correct.

Please go through the code and help me out in the configuration.void i2c_init(void) {  I2C1_FREQR = 0x20;// 16mHz  I2C1_CCRL = 0x50; // 160  I2C1_OARH = 0x40; // 7-bit addressing and add-mode configuration  I2C1_CR1 = 0x01; // enable peripheral}void ...

VSrin by Associate II
  • 2413 Views
  • 4 replies
  • 0 kudos

STEVAL-ISB044V1 cannot communicate with ST-Link V2

Hi all,I'm using theᅠSTEVAL-ISB044V1 evaluation board for the wireless charging test. The evaluation board is based on STWBC-EP and can be programmed with ST-LINK V2. STM8AF6166 is the core of it, so I post here. I tried to program the board, and the...

Dilemma by Associate II
  • 2948 Views
  • 4 replies
  • 0 kudos