Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
HI All,I am facing issue with STM8S103F2 controller Timer1. I am configuring timer1 for 5 sec, but it is giving me interrupt in 10 mili second only. It is not taking my prescaler value. can anyone help me on this, i am putting my code:stm8/ #includ...
I want to know in "ST6210C" controller, IS "Data RAM (084h-08fh)" has non volatile memory ? If it is not, then please tell me which memory space in "ST6210C" controller is non volatile ?Regards,Hitesh
hi,every one. i am working on Bootloader with STM5288 and STM6266 microcontrollers in PC application Side(I am making own PC application as per my user interface),So what are the sequence of commands we need to send from the PC applications,that we c...
I was using STM8SVLDISCOVERY in a small project because it was the evaluation board that I had, but in a more final stage I would like to use an stm8sl001j3 as uC.For that, I got a STM8-SO8-DISCO to be able to use the same uC that I want in the final...
I am trying to obtain the gerber data for the above device on here, but cannot seem to find it, I have the recommended footprint pad size, but want to see how the device has been tracked away from the 0.19mm pads
Hello!My company is engaged in manufacturing oftelephones And we are looking for supplier of this detail supressor P6KE 12CA GP909And we could make an order for that suppressors if itshould suit us And it's very important to know for our engeneers wh...
Hello,Using STM8L050j3, ST LINK/V2 ISOL, STVD.I am studying the UART and i have connected MCU and ST LINK/V2 ISOL.They use SWIM with USART TX / RX Pin.A problem is that PC don't receive the any text.I think that cording is fine(easy example) but i s...