Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to solve this error???

i am adding stm8s.h header file and getting this error.i dont understand why i am getting this error.errors are...Compiling main.c...cxstm8 -i"..\..\..\..\..\..\..\..\program files\stmicroelectronics\st_toolset\include" -i"..\..\..\data manual\stm8s...

MAnsa.1 by Associate II
  • 2234 Views
  • 2 replies
  • 0 kudos

How can I maximize or optimize the range of voltages the ADC can sample for a highly sensitive system?

Let me start by providing a little background on my project. I'm working on developing an avalanche transceiver. For those of you who are unfamiliar with avalanche transceivers, an avalanche transceiver is a search and rescue device used to help loca...

SCutl.1 by Associate II
  • 2316 Views
  • 5 replies
  • 0 kudos

Hii I want to turn ON LED

i have positive and negative voltage in the range of 1000v.i connected one LED to indicate minus voltage.led is connected to PD1 of stm8s003f3 controlleri put this condition....#define SevenSegmentDisplays_GPIOD_ODR_ResetValue 0x7E#define SevenSegme...

MAnsa.1 by Associate II
  • 1192 Views
  • 2 replies
  • 0 kudos

High Voltage Pulse Discharge

I would like to discharge my capacitor at high voltage(1200V). The load will reach 1000 A about 150-200 ns, and ring down. In order to switch that capacitor, i need high di/dt switching device. SCT50N120's diode is fast enough for my application, but...

OKula.1 by Associate
  • 1645 Views
  • 3 replies
  • 0 kudos

src0 and stm6600

1.what is difference between Src0 and Stm6600? One thing I could notice is the ton_blank time.2.Why ton_blank time has a range?for example min 1.4, typ 2.2, max 3.03.What value should I consider when selecting one?

letgo04 by Associate
  • 771 Views
  • 0 replies
  • 0 kudos

How to configure the TLI interrupt source to the stm8s003k3 and how to clear the TLI interrupt source .

Hai ,Here I am using the STM8S003k3 micro-controller. In my project , I want to configure the TLI interrupt source .please any one can help me how to configure the TLI interrupt source .Or can any one help one help me how to disable the external pend...

Trinu by Associate III
  • 771 Views
  • 0 replies
  • 0 kudos

Resolved! STPTIC tunable capacitor DC Ground

Hi.I have the STPTIC-82G2 tunable capacitor, and I have noticed that there is no ground pin. What is the DC ground that the bias pin is referenced to? Should I provide DC ground through RF1/RF2 pins?Thank you!

KTrot.1 by Associate II
  • 3052 Views
  • 7 replies
  • 0 kudos