Flash Controller BTU
Is it necessary to execute the flash controller instruction BTU of the ST10F269 out of internal flash or it can be executed from RAM or external memory.
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Is it necessary to execute the flash controller instruction BTU of the ST10F269 out of internal flash or it can be executed from RAM or external memory.
hello sircan someone, help me with that "SUB SP,#$9 " ,with is mentioned in the LATEST PROGRAMMING MANUAL OF STM8S PAGE 151.if you write that in an even very 1line program, you have an errorCan't match Addressing mode ' SUB SP,#$9'is there a n er...
hello sira very simple asembler program ,with a big problemits in ST visual develop , with the inside st assemblerthat simple program ldw X,#stack_end ldw SP,X PUSH $C SUB SP,#$02gives that error Error 54: Can't match Addressing mode ' SUB SP,#$02'...
From the drawing of DocID28549, PIN22 of the evaluation board (STEVAL-ISA164V1) is described as UART_Tx and PIN23 is described as UART_Rx, but if you search for UART in the attached source file, PIN17 and PIN18 will be searched.Which part of the atta...
The diode is used in a boot strap circuit. Thanks
could you tell me MTBF and FIT for part M24256-BFDW6TP,
I've just opened this issue on ST X-CUBE-EEPRMA1 github repo.All that commented lines sound suspicious to me.I'm not sure that the driver is production-ready, It seems an interanl work in progress.