2023-08-29 4:58 AM
We are using SPINFamily Evaluation Tool 3.2 with EVLPOWERSTEP01 device for operating the stepper motor. Once we programmed the parameters the stepper motor was running with some speed e.g. 411.37 step/sec but after some time stepper motor step/sec suddenly increased automatically and at that time SPEED register was shown as 3906.5 step/sec (independent of human interference) and Status window showing Command error
I have attached a Register map and screenshot for shown SPEED is 3906.5 step/sec.
@
2023-09-27 2:08 AM
Hello @shrikant_swami
Probably a communication error in the firmware that is then interpreted as a Run command.
Let me know if these info are useful to you.