Other: software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STNRGPF01 related questions

Hello, I found a problem in eDesignSuite when i try to use STNRGPF01 (PFC boost interleaved IC).At input current sensing the ICS Target Voltage is 3.00V and in the datasheet the ICS Target Vltage looks like it is 1.25V (also in the Help section of eD...

0690X000006CBzZQAW.png 0690X000006CBzUQAW.png

Good morning , I would like to know if it is possible to extract the schematic/ BRD of this component in order to speed my design? Thanks a lot for your help, Kindly, Mailys

As you can see in the picture, I don't the ability to extract with PSpice, furthermore when I save it as .PRJ, after downloading Orcad, if I try to open the .PRJ there is nothing but a text file inside. Text as below of the Prj file : <eDesignStudio ...

mCAZA by Associate
  • 446 Views
  • 1 replies
  • 0 kudos

can't connect the X-NUCLEO-GNSS1A1 via I2C

stm32 board: stm32f446reHi, recently, I bought the expansion board X-NUCLEO-GNSS1A1, and I've managed to communicate it with USART. However, I have a hard time to do that with I2C, it stuck at slave address transferring. In the beginning, I thought t...

0690X000006CKmBQAW.jpg
PTsen by Associate III
  • 340 Views
  • 1 replies
  • 0 kudos

Why pfc is not working

I have used stm l4984d ic for pfc control and got all the necessary parameters within range but still no pulse is generated by pfc ic. What can be the possible errors In my design so that I can rectify them

JDar by Associate
  • 348 Views
  • 0 replies
  • 0 kudos

How can I program the EVAL-IPFC01V1?

Posted on February 20, 2018 at 13:48Yesterday I started to work with the EVAL-IPFC01V1.Can I program the STNRGPF01 with the ST-LINK/V2 through the SWIM connector J2?Or I must use the UART J3 with the adapter in the box? In this case what is the corr...

We need your assist and solve for quality issues of ST's IC (L7812CV-DG), according to our client's feedback which kind of defective IC(no voltage drop value and no voltage output) is always add.

There are our test and verify procedure of defective IC as following:Our terminal client found IC function disabled issues(no voltage drop value and no voltage output) and feedback------- engineer found disabled IC through confirmation and analysis( ...

ALI.30 by Associate
  • 379 Views
  • 0 replies
  • 0 kudos