2008-01-01 07:58 AM
2004-12-02 08:04 PM
Hi to all
I have a problem whit writing in to flash. My code is in flash (Sector B0F0 to B0F4). All the routines for wrtiting in flash is executed from RAM (flash.o execution is mapped at address 0x20000000 in scat file). I write the sector B0F5 to B0F7. When i execute step by step the code work fine, but in normal run mode the micro stop at undefined address. The problem is probably the 0x6E000010 code returned from an access to flash during writing flash operation . . . (??? if an interrupt is activated ? the fw tries to access the flash???) FOr example this is ERASE FLASH routine: void FLASH_EraseSector(dword Xsectors) { volatile dword temp; WaitForLastTask(FLASH_BANK0); WaitForLastTask(FLASH_BANK1); FLASHR->FCR0 |= FLASH_SER_Mask; FLASHR->FCR1 |= Xsectors; FLASHR->FCR0 |= FLASH_WMS_Mask; // while ((FLASHR->FCR0 & 0x6) != 0); // while (((FLASHR->FCR0 & FLASH_SER_Mask) != 0) | // ((FLASHR->FCR0 & 0x06) != 0)); do { temp = FLASHR->FCR0 & 0x00000006; } while(temp != 0); } Can anyone help me ? smart2004-12-02 08:49 PM
Hi smart,
I think that you have forgotten the bit LOCK of the register FLASHR_FCR0. This status bit is very important because we can not access to any register if this bit is set to 1, so just add this line of code after anny access to or from the FLASH: while(FLASHR_FCR0 & 0x16); This line of code should replace the following code: do { temp = FLASHR->FCR0 & 0x00000006; } while(temp != 0); Regards, Bouha2004-12-02 09:22 PM
Hi Bouha,
i have already test this solution . . . but it NOT work: also now the micro stop at undefine address if run normaly and it work fine only if i execute step by step !! tnks for your help smart2004-12-02 09:52 PM
Hi smart,
Please add the to the flash.o (in scatter file) the program which call the flash routines, because this program must be also excuted from RAM. Rgds, Bouha2004-12-02 10:36 PM
Hi Bouha,
i have moved all the calling routines in RAM but . . . it not work . . . the debugger stop and return ''Stopped due to unknown reasons - Stopped at 0x00000008: Line 195 '' (=UndefinedHandler) (note: i'm testing the EraseSector(..) routine...) tnks smart2004-12-03 02:46 AM
Hi smart,
In this time i think that i have the solution to your problem, Please find attached an example which illustrates how to erase a sector then writes some data, this example is executed from the flash sector 0 then erase and write a data to sector 1. This example work fine with my board :) Rgds, Bouha ________________ Attachments : flash_example.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtTJ&d=%2Fa%2F0X0000000aQR%2FKpyYBuoOT.EP5ekOd4vpFfaDKhzxS3wEayU6BqeBTvI&asPdf=false2004-12-03 03:03 AM
Hi Bouha,
tnks for your code. But it is possible execute from B0F0 and write to B0F1 ? In my first tests i have writing data in B0F5 executing code from [B0F0..B0F2] . . . but from Reference Manual (pag. 46, Par. 2.4) i read that: ''... the write operation commands must be executed from the other bank or another memory...'' . It is also possible to write a SECTOR executing code from another SECTOR of SAME bank ? Thanks !! smart PS - now I try your suggestions :-)2004-12-03 03:15 AM
Hi smart,
No, we can not execute code from a SECTOR and write to another SECTOR, but we can do this by executing the code from RAM using the scatter file . Rgds, Bouha2004-12-05 07:18 PM
Hi RISC,
OK, it is clear. . . This is the structure of my application: - B0F0 to B0F4 - Code of application (USB included) - Address 0x20000000 (RAM) : routines for writing in FLASH (B0F5-B0F7) - RAM +0 : other variables (scat file attached) In this situation, when i execute step by step the call to the flash routines work fine, but in normal running the micro stop at undefined address. NOTE - Memory map [....] Execution Region FLASH_RW (Base: 0x20000000, Size: 0x000008ac, Max: 0xffffffff, ABSOLUTE) Base Addr Size Type Attr Idx E Section Name Object 0x20000000 0x00000874 Code RO 350 .text flash.o 0x20000874 0x00000028 Code RO 351 i.FLASH_EraseBank flash.o 0x2000089c 0x00000010 Code RO 352 i.ResetBit flash.o [....] Can you help me ?