Posted on September 13, 2006 at 11:00It's simple, you have just to add the following code line to enable the interrups from the Flash and use the standard library Flash routines (Write & Erase) FLASHR->CR0 |= 0x200000; And in the 71x_it.c file add t...
Posted on September 13, 2006 at 06:05Hi, I verify it and it works fine whith the library flash routines. I guess you aren't using the library flash routines? Rgds, Bouha.
Posted on May 12, 2006 at 06:42Hi, 1) Yes, the very first time means the first time after POWER_ON. 2) There is no limitation on programming the non volatile part of the register. Best regards, Bouha