2006-12-28 09:09 PM
Replacing IGBT's with MOSFET's on STEVAL-IHM003V1
2006-12-03 11:43 AM
Hello,
Would anybody recommend a type of MOSFET that would be suitable to replace the IGBT's with on STEVAL-IHM003V1 power board? I want to run my power board with an input of 15 volts which cant be do without replacing the IGBT's with MOSFET's. Thanks in advance Regards2006-12-28 09:09 PM
The IGBT is an hybrid device which tipically integrate a bipolar transistor to drive a power ''N'' MOS.
This solution concurs to reduce the input capacitance to obtain an high speed power device. The value of input capacitance of a power Mos is inversely proportional to RDS_ON; that means high current device == high input capacitance and consequently low speed (and maybe high temperature to dissipate). So it depends on your application: if You need speed and power You must use IGBT. In any case You must see the board STEVAL schematic for actual IGBT command logic and evaluate the compatibility for a direct gate MOS command. Sixtus 🙂