2005-11-08 10:02 PM
RAM debug macro files for JLINK and IAR compiler
2005-10-31 10:03 PM
Does any one have a macro file, to enable RAM debug when using JLINK and IAR compiler?
Or is there another way to get RAM debug to work in IAR. Best regards, Frank Andersen2005-11-01 12:40 AM
I have the IAR ver 4.30A, and a JLINK kicstart and kit with the STR711 from IAR. The problem is that all the examples are programmed into flash, if I select the configuration file to the Linker to xxxxx_ram.xcl, then the code is not excuted from RAM.
For the Atmel SAM7 there is a macro for Debugger, to be used when debuging in RAM, that is file I am looking for to the STR71x Best Regards, Frank Andersen2005-11-07 12:54 AM
Hi,
I'm using winIDEA with IAR, but I think you should uncheck the flash loader box, Manu ________________ Attachments : iar.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOo&d=%2Fa%2F0X0000000aPT%2F7YLgQQsWEgqWPSY0t7LWT0iLhemmHIeLIQvBl90D_f0&asPdf=false