2006-03-20 10:19 PM
JTAG cannot stop target, what's the problem?
2005-11-17 02:17 PM
Any guys can tell me why JTAG unable to stop the target, error number is V2001B? It is STR710-EVAL board. Is there any problem in reset line?
Thanks.2005-11-22 11:54 AM
Thanks gentlemen, my hardware guy changed the chips and this problem disappeared. So if JTAG reports this problem, it should be chips issue.
2006-03-12 10:16 PM
Is there any possibility to reset the MCU?
I have the same Prob like dawei. Every time i want to connect to the STR710-Eval Kit the RVDEBUG connection tels me that the device is held in Reset. an after that Device error V2001B. can you plz give any advice. thx. bye re-G EDIT solved: RVEMI is gone :-[ \EDIT[ This message was edited by: re-G on 13-03-2006 12:33 ]