Skip to main content
Associate II
November 23, 2024
Question

Programming STM with SWV without nRST pin

  • November 23, 2024
  • 0 replies
  • 365 views

Hello,
I am programming STM32G491, while I need to use nRST as GPIO (MCO). I am using a code that you can see below. The problem is that when I am debugging a program, the debugger is disconected after HAL_FLASH_OB_Launch(); (this should reset MCU, am I right?). What can I do with that? I do not have a UART on my board, so SWV is my only option here...

Thank you for response.

 

 

 

SystemClock_Config();

 

/* USER CODE BEGIN SysInit */

HAL_Delay(5000);

HAL_FLASH_Unlock();

HAL_FLASH_OB_Unlock();

OBInit.OptionType = OPTIONBYTE_USER;

OBInit.USERType = OB_USER_NRST_MODE;

OBInit.USERConfig = FLASH_OPTR_NRST_MODE_1;

HAL_FLASHEx_OBProgram(&OBInit);

HAL_FLASH_OB_Launch();

HAL_FLASH_OB_Lock();

/* USER CODE END SysInit */

 

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_SPI1_Init();

This topic has been closed for replies.