cancel
Showing results for 
Search instead for 
Did you mean: 

ST-link stop working after configuring ST32H7 as USB Device

GioBytem
Visitor

Hello everyone,

I'm trying to debug firmware on a custom ST32H750XBH6 board. Once I configured the MCU on StmCubeMX to act as a USB_OTG_HS after flashing the firmware the ST-link stopped working and it gave me the error message:
Target no device found:
Error in initializing ST-LINK device.

Reason: No device found on target.

 

It is strange because the same thing happened with a NUCLEO-G0B1RE. After configuring the board as USB_OTG_FS and flashing the firmware, the st-link embedded on the board stopped working. I'm sorry if this was a well-discussed topic, but I couldn't find an answer in the community, I'm an early developer.

Thank you in advance.

0 REPLIES 0