2005-11-29 01:13 AM
how to program STR710 with GNU tools?
2005-11-12 04:07 AM
Hi..
I have a new STR710 EVAL board which comes with the RealView ICE. I plan on using uClinux on the board. I have a linux image to upload to the unit. However, I don't know how to actually download it to the dev board. What tool do I use? (For instance I've used avrdude when programming atmel processors) I don't have the realview dev suite and would preferably perform all operations from within a linux environment if possible. Any and all help is appreciated. kodge2005-11-29 01:13 AM
Hello, did you ever find a solution to this?
The above links as far as a ican tell are all propreitry windoze tools, and as such not much help for proragramming in linux. To boot windoze every time would be a real pain, and is unacceptable. I'm looking at some software that was written to reprogram some pda bootloader and also a programmer for the lart pcb, which it might be possible to adapt as neccasary. Any help here much appreciated. http://handhelds.org/cgi-bin/cvsweb.cgi/debrick/bsrflash/ http://www.lart.tudelft.nl/projects/jtag/ Thanks Dan [ This message was edited by: dan2003 on 29-11-2005 16:22 ]