2020-10-30 08:09 AM
I can't find any forum for the Teseo so I'm asking here. I need to know if it's appropriate for a very sensitive receiver in the sub-200MHz range. If the module contains any DC/DC switches that raise the noise floor in these frequencies then it's a non-starter for my project.
Furthermore, because of the mechanical size constraints, proximity of the module to the RX chain of the circuit is non negotiable, so I can't just redo the layout to move it away.