2004-03-15 10:20 PM
2004-03-15 10:20 PM
Hello All ,
This is a very important and urgent issue for us. I think you can solve it swiftly for us. From the measurements it seems that the signal does not conform to the standard. The horizontal synch is 2.855 microseconds instead of 2.092 microseconds The horizontal frequency is 48.92 kHz instead of 48.636 kHz . The vertical synch is 163.6 microseconds instead of 124 microseconds Those settings are related to the HWCRTC_pucMonitor1024x768 ,which includes the cr registers. Most probably the cr1 to cr5 settings have to be adjusted . Please send us the correct settings ASAP. Thanks Latino from Israel