Posted on May 17, 2011 at 12:10Hello I have a problem with ports A & B when I'm running it on the DK3400. The attached program is a timer2 interrupt that toggles all PORTA from 0 to 1 .On the main I'm writing 0 and one to PORTA and it changes states...
Posted on May 17, 2011 at 12:10Hello Support Regarding the 80 pin package on the uPSD33xx that have dedicated pins for A8,A9,A10,A11 as we know the the uPSD33xx is compatible to the uPSD34xx but in the uPSD34xx those pins are NC !!!!!!!!!!!!!!!!!!!!...
Posted on May 17, 2011 at 12:09Hello Support , Could you send me some links or code examples / apps.notes how to use the external memory interface with uPSD33xx family ? Thx Amir
Posted on May 17, 2011 at 12:08Hello All , I saw on the schematic of the DK3300 there is PS/2 Connector . Pl's advice if i can get a demo software for it ? Thx Amir Sherman
Posted on May 17, 2011 at 12:05Hello , I have a technical question: how can I produce a signal using a timer in the CPLD. I wont to extend the signal of the PWM in the CPLD using a timer. Latino